(0)| 8/31/2012 3:12 AM | |
|
Joined: 11/30/2007 Last visit: 1/13/2026 Posts: 12 Rating:
|
Dear Sir Our client using IP 241 with MFLB 6ES5241-1AA11 and adapter paralel input BCD. Their program are not using standard FB to read actual value IP 241 (The standard FB only for synchronize) . Instead using FB 157, their program using load transfer peripheral ( FB 160 for channel 1 & 2 card no 1). Would you share anyone to us how this technique program are implemented by giving explanation the logic inside FB 160. Thanks & Regards, Bayu AttachmentF:\PIC S5 INDOPORLEN\IP 241 Logic.zip (416 Downloads) |
| 9/2/2012 1:12 PM | |
|
Posts: 1742 Rating:
|
Hello, Have a look to chapter 10.12.7 in this manual. http://support.automation.siemens.com/WW/view/en/16739885 They explain in that cahpter the principle of reading values using I/O adressing. Firts is to know what are the start I/0 address used for your IP241. |
Follow us on