9/13/2012 10:23 AM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello, click in the LAD/STL/FBD editor with the right mouse on the SFB35 and select "Special Object Properties > message..." from the context menü. Here you can for each message identifier (SIG 1 up to SIG 8) change the message class. If you click in the message class, you will receive a menü for kind of messages (example Alarm-high, or Warning high, ...). After you have to confirm with OK. http://support.automation.siemens.com/WW/view/de/21480564 With best regards |
9/17/2012 6:42 PM | |
Posts: 3 Rating:
|
Thanks a lot Cicero |
Follow us on