(0)| 9/17/2012 11:11 PM | |
|
Posts: 4 Rating:
|
HALLO! I'm having the following problem: In the WinCC Explorer to open the settings editor AlarmLogging classes and types are lost. The Alarms messages generated automatically lose your settings. However, if you change the property "Computer Name" of the WinCC Explorer, the editor AlarmLogging now functions correctly with your settings (classes, types, messages Alarms). A possible cause of this strange behavior of the "Alarm Logging" can be ran by mistake because the runtime in engineering station. Performed the procedure on the link below, but got no success. Is there any other procedure for solving this problem? Look this attach information: PCS7 V.7.1 using the library CEMAT V.7.1 1 ES 1 OS Server Redundant 3 OS Clients AttachmentAlarmLogging.zip (78 Downloads) |
| 9/20/2012 5:25 PM | |
|
Posts: 836 Rating:
|
Did you try to recompile the OS? |
Follow us on