(0)| 9/26/2012 9:20 PM | |
|
Posts: 4 Rating:
|
I have a couple of C7-635 Key's that are running the same PLC and HMI (WinCC Flex) programs. Both are continuously cycling through the date/time in Windows CE and I can not set it . However, if I look at the PLC clock through Simatic Manager/Module Info, it shows the correct date and time. The problem is the date and time are displayed in the HMI program, and it's gibberish. Are there any configuration issues which could cause the clock to function incorrectly? I've attached two small videos showing the issue.
AttachmentC7-635 Clock.zip (163 Downloads) |
| 10/1/2012 1:20 PM | |
|
Posts: 3037 Rating:
|
Hello dptrw, Which version of WinCC flexible do you use? Do you use an area pointer for date and time synchronisation? Tweety |
Follow us on