(0)| 6/22/2012 12:54 PM | |
|
Posts: 139 Rating:
|
Hello, colleagues. In this documentation I can read "Note. The operating system update is only possible using a serial cable." (chapter 13, page 13-1). In this documentation I can read "When performing an operating system update, you can use all the communication connections supported by your operator panel." (chapter 2, page 11). So I cannot understand have I to use serial cabel for OS update for OP270 10"? Best regards, SpKV. |
Last edited by: SpKV at: 6/22/2012 12:56 PM |
|
| 6/22/2012 1:17 PM | |
|
Joined: 4/24/2006 Last visit: 1/16/2026 Posts: 9105 Rating:
|
Hello SpKV, Please have a look at this link: What transfer options are available in the various operator panels? Best regards, Wizard |
| 6/25/2012 9:51 AM | |
|
Posts: 139 Rating:
|
Thank you, Wizard for answers. Did somebody successfully used USB->serial convertors in real practice? Do you know so experience? TIA, SpKV. |
| 6/25/2012 10:19 AM | |
|
Posts: 3037 Rating:
|
Hello, The transfer does not work with USB serial converter. You can see this information in the following link. What transfer options are available in the various operator panels? Tweety |
| 6/25/2012 1:57 PM | |
|
Posts: 3037 Rating:
|
Hello, I have heard from colleagues, if you have luck, then the USB serial converter can work, butthis converter does not work always. You should use PROFISBUS as transfercanal at OP270. You need a CP for your computer. See the following FAQ. How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Tweety |
Follow us on