(0)| 11/10/2012 6:23 AM | |
|
Posts: 1064 Rating:
|
with the profibus cb it use's profibus protocol not uss but you can connect all three to a pc using profibus protocol and starter software here is a link to the manual if you require it http://support.automation.siemens.com/WW/view/en/6586565 |
Last edited by: playerslight at: 11/10/2012 6:31 AM |
|
This contribution was helpful to
|
|
| 11/10/2012 6:46 AM | |
|
Posts: 1064 Rating:
|
to connect to a pc using profibus you do need a cp card in the pc . to use uss from pc to mm440 you can use a pc kit and connect them .I am not sure about connecting 3 on uss i have never tried it . I have used uss to connect to 1 at a time but is slow compared to profibus. after reading the manual for multiple mm440's you have to use rs485 not rs232 protocol .here is the link to the manual http://support.automation.siemens.com/WW/view/en/24178253 |
Last edited by: playerslight at: 11/10/2012 7:00 AM |
|
| 11/28/2012 10:02 AM | |
|
Posts: 13 Rating:
|
Thanks!, i'm working on the project right now i'll publish the results when i'm done. |
Follow us on