(0)| 11/15/2012 4:24 PM | |
|
Posts: 6 Rating:
|
Dear Experts, requst your support for similar problem,(mm440-Fan application) for one of our customer for avoiding under voltage while small dip we activated the KIB.But one of the drive started tripping on over voltage.We reduced the Swith on level kinetic buffering (p1245) to 69% still drive is tripping in over voltage. I am notable to understant the issue.More than 300-400 v boosting in short time.Is it possible to control the voltage. Backup attached here. form the back up it is found that the slip r0330 is 31.33.It will effect anywhere in KIB.At what rate drive will reduce the running frequency while KIB enabled. Please support Thanks in advance ABHI AttachmentBackup.zip (166 Downloads) |
Last edited by: O_Moderator at: 11/19/2012 11:26 AMnew subject after splitting from /tf/WW/en/Posts/61215#top |
|
Follow us on