(0)| 5/17/2007 9:09 AM | |
|
Posts: 177 Rating:
|
Files attached. The triggers for the alarms are not from Step7, but from an external application where the tags are passed via OPC. All processes were saved prior to the message tags being 'lost' Regards, henno2000 Attachmentdiagnose.zip (241 Downloads) |
| 5/17/2007 1:31 PM | |
|
Posts: 1275 Rating:
|
Hi, When you said -->I was contacted to discover that almost every alarm had been activated. Upon further inspection the plant was OK, so alarm logging was examined and found that most of the message tags for the alarms had disappeared and replaced by blanks. Well.. for the alarms to be activated the tags must've been there at that time... But then you said the tags had disappeared,.. that's the MessageTag column in Alarm Logging, right? Does that apply to the analog alarms limit checking? Has the limit checking gone away all together, as if you had never configured that? About the logs, here we go: OPC log: 2007-05-03 10:06:05,578 ERROR FOPCData::AddWriteItems m_dpOPCItemMgt->AddItems(1, 058cff08, 037dfab4, 037dfaa8)- ERROR 00000001 2007-05-03 10:06:05,578 ERROR - ChannelUnit::SysMessage("[OPC Groups (OPCHN Unit #1)]![DMS_MachineGuard_C430]: AddItem "MCG_C430ConveyorLH2NAME02" failed, error=c0040007 (The item is no longer available in the server address space)") 2007-05-03 16:35:55,921 ERROR FOPCData::GetStatus- ERROR 800706ba 2007-05-09 13:15:06,734 ERROR FOPCData::GetStatus- ERROR 800706ba 2007-05-09 13:15:49,000 ERROR ..FOPCData::InitOPC CoCreateInstanceEx- ERROR 800706ba 2007-05-09 13:15:49,015 ERROR - ChannelUnit::SysMessage("[OPC Groups (OPCHN Unit #1)]![DMS_MachineGuard_C430]: CoCreateInstance for server "National Instruments.LookoutOPCServer" on machine AIMM-WINCC-WS03 failed, Error=800706ba (HRESULT = 800706ba - RPC_S_SERVER_UNAVAILABLE (The RPC server is unavailable.))") PDLRT log: //==================================================================== // WinCC reported exception with code: C0000005 ACCESS_VIOLATION // Date: 09.05.2007 - Time: 21:15:45 // Caused at logical address 00429ADA 01:00028ADA --> This just means the script engine has crashed. S7 Protocol Suite log: 2007-05-09 22:19:38,156 ERROR Illegal tag address "C-210_YA_1200A.Value"! System log: 255,09.05.2007,00:15:01:640,1012252,4,,AIMM-WINCC-S001,ArchiveManager,Backup:invalid path C:\WinCC Projects\ABP-HIT2-master\CommonArchiving\* ! 255,10.05.2007,10:19:08:250,0,4,,AIMM-WINCC-S001,ArchiveManager,Failed to switch archive(Type:1):(null) ! --> Check this out. Best regards, Danielle |
Last edited by: Danielle at: 17.05.2007 13:49 |
|
Follow us on