(0)| 12/21/2012 11:39 AM | |
|
Posts: 8092 Rating:
|
Hello, From your query description, I presume as follows. You have configuered drive by setting P083 = 3 as armatuer feedback. But in this case speed is not controlled & motor runs at full speed. If you set P083=1 & tacho is connected, the speed of motor is controlled. So I guess that you want to know why the speed doesn't controll with armatuer feedback? Assuming this is your question, please find attached here with the sheets which gives the information about feedback. When you set P083=3, please check the value in P115 value.Moreover does your motor run in field weakning mode? If motor runs fine with tacho feedback, why you want to set armatuer feed back? AttachmentFeed back device configuration.pdf (290 Downloads) |
Follow us on