(0)| 1/7/2013 5:14 PM | |
|
Posts: 23 Rating:
|
hi, on a pc is it possible to connect and simulate a masterdrive (it may be abb acs800 drive)andstep7 program thatare connected over profibus? thanks. |
| 1/7/2013 5:21 PM | |
|
Joined: 1/28/2009 Last visit: 1/5/2026 Posts: 6892 Rating:
|
Hello, If I understand your case, You have a PROFIBUS Slave and want to test the functionality.If I am right and you do not have access to a PLC,You can try a PROFIBUS Master Simulator which can generate exact telegram a class1 master generate based on the provided GSD file.Take a look at here: Profibus-DP/DPV1 Best regards Hamid Hosseini |
Follow us on