(0)| 1/9/2013 3:29 AM | |
|
Posts: 1 Rating:
|
HI Friends Currrently i Am doing a Project with S7-200.The CPU i am using is 226 CN. I have prohrammed the PLC as SLave thru MODBUS_init and Slave instructions. I dont have the library installed in my Step-7 Microwin. I just copied it to my Program. I am using MODSCAN to scan the outputs in my PC. But the modscan cannot communicate with the PLC.It is giving a 'Timed Out' message. Anybody can pls help? Pls find the PGm Attached.Do we need to install the library function in step-7 for the instruction to work? regards chit AttachmentA268_Modbus.pdf (358 Downloads) |
Follow us on