(0)| 1/24/2013 11:28 AM | |
|
Joined: 10/11/2006 Last visit: 1/29/2026 Posts: 6077 Rating:
|
Dear Mr. Moreno, Did you sent one of these drives to the repair service in order to see what is defective? Please check the line supply for voltage peaks and the frequency. (200 ... 240V AC, 47 ...63 Hz are allowed). At the output side check the equalisation of the potential between the converter and the motor as well between the control and the converter (analogue source). Please find the EMC rules: http://support.automation.siemens.com/WW/view/en/60612658 Best Regards |
|
With best regards, |
|
Follow us on