(0)| 1/29/2013 12:22 PM | |
|
Posts: 391 Rating:
|
Hello, please take a look at the Documentation http://support.automation.siemens.com/WW/view/en/64930686Chapter 1.1.2 Some examples: R0=3.5678 R[1]=-37.3 Z=SQRT(R1*R1+R2*R2) |
Last edited by: APC Tech Team at: 1/29/2013 12:23 PM |
|
| 1/29/2013 4:00 PM | |
|
Posts: 391 Rating:
|
Sorry, I misunderstood your question. Yes, in ISO mode (named "ISO dialect" in the Siemens documentation) R parameters cannot be used. I think that the only thing you can do is to switch back and forth from Siemens mode to ISO mode with G290/G291. In Siemens mode youdo the calculations with the R parameters and assign the result to the system variable $C_MACPAR that you will use after in ISO mode. Please look at the $C_MACPAR in the Function Manual ISO dialects http://support.automation.siemens.com/WW/view/en/65371498chapter 2.3.3 The problem is that you cannot write from ISO to $C_MACPAR but you can only read in ISO what is written in $C_MACPAR. So it is a read-only mode. |
| 1/29/2013 4:58 PM | |
|
Joined: 9/10/2007 Last visit: 1/21/2026 Posts: 71 Rating:
|
Dear APC Very good your suggestion. Thank you for your reply. |
Follow us on