(0)| 1/25/2013 9:05 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
With MMC (Micro Memory Card) slotted, why does the STOP LED blink on the SIMATIC S7-300 CPU? |
| 1/25/2013 4:15 PM | |
|
Posts: 4620 Rating:
|
Hello cy429 Your MMC is original SIEMENS? |
| 1/29/2013 10:40 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello cy; An FC is a block of programming code, so this problem could have nothing to do with the hardware configuration. I would expect that the number of the "missing" FC is inluded in the diagnostic buffer message, and also the OB required to handle that type of error (probnably OB121, "Programming error"). The presence of that diagnostic OB in the CPU program allows the PLC to run even with the SF LED active, and gives you time to correct the error (locate the missing FC and download it to the PLC program in this case).. Using the diagnostics buffer of the SIMATIC S7-CPU Which organization blocks do you need for error handling? Could you copy the complete message (or your diagnostic buffer messages) to this thread po we may examine it and maybe give you more ideas? Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 1/29/2013 10:41 PM |
|
| 1/29/2013 10:46 PM | |
|
Posts: 33 Rating:
|
Hello Daniel, thanks but How about the memory I used 512 KB MMC? is it correct? |
| 1/29/2013 11:12 PM | |||||||||||||
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello cy; Depending on the version of CPU 312, it was loaded with a work memory of 16 or 32 kB. See these Product Support pages:
So with your 512 kB load memory you are well in the clear. How can you obtain an overview of the memory concept of SIMATIC S7-300 CPUs and C7 devices? Hope this helps, Daniel Chartier |
||||||||||||
Last edited by: dchartier at: 1/29/2013 11:13 PM |
|||||||||||||
| 1/30/2013 8:29 AM | |
|
Posts: 4620 Rating:
|
Hello cy429, Copy the entire contents of the diagnostic buffer and send it. Ste |
Follow us on