(0)| 2/1/2013 9:00 AM | |
|
Posts: 455 Rating:
|
Hi, the keyword is "Interface description" e.g. here a link for a SIN810 GA1. Please find the link by Yourself, pending on the target hardware. Basically You have to open the PLC-program (S5-Tool needed) and than You have to look for the corresponding Bits in the documentation. Now You can try to trace inside the PLC-program the signal(s). Without S5-Tool (program) no access to the content of PLC-program. Without S5-Tool You can debug only PLC-Input/Output/Flag-Signals in PLC-Status from the CNC-Screen. (It's pending on CNC-Type and configuration) But NO ACCESS to the PLC-logic. |
Follow us on