(0)| 2/6/2013 6:32 PM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
The correct procedure is by selecting one project, preferable the OS project, since the pictures will make the plant hierarchy. Select the project and right clickand search for "update in multiproject" (its behind the Charts folder I believe). Now the hierarchy of the other project or projects will be updated after clicking ok. If done, you can see small shortcut icons in the hierarchy folder names. so you known that that project is updated. I dont believe exporting projects one to another is the right solution....at least according what you need to do here. |
Last edited by: Oreca at: 2/8/2013 11:43 AMSelect project, right click->Plant Hierarchy->Update in multiproject If I could help you, you can use the RATE button. Thank you. |
|
Follow us on