(0)| 2/8/2013 2:48 PM | |
|
Posts: 975 Rating:
|
Can ET200SP be used on Simotion? I cannot find it in the hardware catalog |
| 2/8/2013 3:22 PM | |
|
Joined: 5/12/2006 Last visit: 1/20/2026 Posts: 22829 Rating:
|
Hello, have you installed the GSD Files for ET200SP ? Regards Christoph |
| 2/8/2013 3:28 PM | |
|
Joined: 9/27/2006 Last visit: 1/20/2026 Posts: 12481 Rating:
|
Hello David; I agree with Christoph: SIMATIC ET 200SP ET 200SP distributed I/O system ConfigurationThe ET 200SP is mounted on a mounting rail and consists of: · An interface module that communicates with all IO controllers that behave in accordance with the PROFINET standard IEC 61158 · Up to 32 I/O modules that are connected to passive BaseUnits in any combination · A server module that completes the configuration of the ET 200SP You will be able to download the GSDML file for the ET 200SP from this link: PROFINET GSD files : ET 200SP Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 2/8/2013 3:34 PM |
|
Follow us on