(0)| 3/9/2013 5:50 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello cromerofs; Have you used the Device Integration Manager to determine which version of the EDD file you are actually using for youe flowmeter? You might have trouble with version compatibility. It is difficult to give you specific help if you do not escribe the equipment you are connecting to the PA network, and the version opf the EDD files used in your earlier version ofPDM. Look at the following links for further information on the subject. SIMATIC Process Control System PCS 7 SIMATIC PDM 8.0 Information about the Device Description Library "SIMATIC PDM Device Library 1#2012" Device Library 1#2012 for SIMATIC PDM Available for Download |
Follow us on