(0)| 3/20/2013 8:03 AM | |
|
Joined: 1/28/2009 Last visit: 1/5/2026 Posts: 6892 Rating:
|
Hello, For the first question, I hope you mean how to generate pulses in internal memories(contrary to send them to output modules).I just know 2 methods to generate pulses in S7 200.Using SM0.5 or using 2 timers (On delay and off delay timers) for generation pulses.It is also possible to enable pulse generation by any binary signal by combining them with an AND binary operation. More information available here. I hope that helps. Best regards ![]() Hamid Hosseini |
| 3/20/2013 6:15 PM | |
|
Posts: 2 Rating:
|
Hi, thanks for your help. I am going to explain what i want to do. i have 2 barrier gates (amano Agp 1700), 2 semaphore (red and green) and 2 loops each loop for each gate, 2 relays (24 vcd) , all for control access in one street. with the loop, i send a voltage to a relay (just to turn on) and i send an input to plc 222 (I0.0), if the second gate is not detecting a cart, the program send an output (Q0.0) to a card that together with the relay,change lights from red to green. But my gate is still down, and for open the gate i need a signal, not voltage. I was thinking if i could sent signal pulse from Q0.0.? I am sending you a design. AttachmentDIAGRAMA.pdf (280 Downloads) |
Follow us on