(0)| 3/19/2013 11:40 AM | |
|
Posts: 3037 Rating:
|
Hello, Here you can find more information about barcode scanner. How can you use an operator panel to output a variable text input as barcode on a printer? Which hardware can be connected to the USB port on Windows-based panels? Tweety |
| 3/19/2013 12:58 PM | |
|
Posts: 5 Rating:
|
Thanks for the reply Tweety. Unfortunately, I've already read those FAQs and couldn't extract help for solving my problem in specific...
|
| 3/22/2013 1:17 PM | |
|
Posts: 3037 Rating:
|
Hello, Which Barcode scanner do you use? Please note, only use barcode readers which convert the barcode internally into an ASCII keyboard code. The current carrying capacity of the USB port differs depending on the type of operator panel. Refer to the relevant device manual in each case for precise specifications. It might therefore be necessary to provide an extra power supply for the device connected, for example, via the Industrial USB Hub 4. See the link.Which hardware can be connected to the USB port on Windows-based panels? Tweety |
| 3/25/2013 5:33 PM | |
|
Posts: 3037 Rating:
|
Hello, Or you use another barcode scanner with USB interface. Which hardware can be connected to the USB port on Windows-based panels? The interface on the TP277 is not a RS232 interface. SIMATIC HMI Bediengerät TP 277, OP 277 (WinCC flexible) Tweety Connecting a Scanner / Barcode Reader to the Integrated PtP Interface on the CPU S7-31xC |
Last edited by: Tweety at: 3/25/2013 5:38 PM |
|
Follow us on