(0)| 3/25/2013 1:35 AM | |
|
Joined: 6/4/2008 Last visit: 11/25/2025 Posts: 1521 Rating:
|
Hi, Manuals can be foundHEREfor the different T400 cards. It is normal for the 3 LED's to flash. If you have a T400 card with custom written firmware (program), then you definately need the original program, because YOU ABSOLUTELY CANNOT upload the firmware. For example, if you replaced a custom T400 or wanted to download the firmware again (Using the DUST1 protocol) What you can do however, is upload the parameters for both the drive and the T400 card. These ARE ACCESSED on the CU card of the drive. //Edit If you had say an "Axial Winder" T400 card, then it would be relatively easy to replace the T400 card (like for like). All you would need to do is to download the parameters again. Be careful and read well !! Regards, Graeme |
Last edited by: Graeme at: 3/25/2013 6:52 PM |
|
Follow us on