(0)| 4/9/2013 1:17 PM | |
|
Posts: 76 Rating:
|
Hello! Can someone tell me if I can configure on that CPU two IP addresses? Best regards Lesko |
| 4/9/2013 2:58 PM | |
|
Joined: 10/7/2005 Last visit: 1/19/2026 Posts: 3054 Rating:
|
Hello lesko No, you can not have two IP addresses on the IM151-8 CPU. It's three Ethernet ports are simply part of an inbuilt 4 port switch (the 4th port is internally connected to the device itself which can only have one IP address). I hope this helps |
|
Cheers |
|
Follow us on