(0)| 5/6/2013 9:18 AM | |
|
Posts: 7 Rating:
|
Please help because it can prevent an unnecessary replacement. |
| 5/8/2013 4:04 AM | |
|
Posts: 7 Rating:
|
This is the program that i still working on it. This project is the upgrade-type so it's very hard to do since i'm not the one who start it from the beginning but i've changed like 70-80% of the program to meet the new requirement. I used to work with newer PLC like Allen-Bradley's ControlLogix, compactlogix...and they're very user-friendly, now working with s7-200 is a mess for me. It's a possibility that i'm not a good PLC programer too. Please look and give me some advice. Thank you so much.
AttachmentPLC-06052013.zip (315 Downloads) |
Follow us on