(0)| 5/24/2013 2:32 PM | |
|
Joined: 10/11/2006 Last visit: 1/16/2026 Posts: 6068 Rating:
|
Hello,
there are no special function blocks for your request. I think, as long, as the on command is given, the actual speed has to be the set on the several setpoint sources, e.g. the ramp function generator p1144 and take it over. Or via the free function blocks and analog value memory. Use therfor the function diagrams in the list manual. http://support.automation.siemens.com/WW/view/en/70983838 |
|
With best regards, |
|
Follow us on