6/23/2013 1:52 PM | |
Posts: 664 Rating:
|
Hai All, Can anyone please share the DriveCLiQ cable Connection Architecture from controller to Keyboard and PP 72/48D PN and Drive .. Thanks&Regards, Raj |
6/23/2013 4:01 PM | |
Posts: 2964 Rating:
|
Hello, Abbreviation for DRIVE CLIQ is "Drive Component Link with IQ". Communication system for connecting the various components of a SINAMICS drive system, such as the → Control Unit, → Line Modules, → Motor Modules, → Motors and speed/position encoders. DRIVE-CLiQ is based on Industrial Ethernet using twisted-pair lines. The DRIVE-CLiQ line provides the send and receive signals, as well as the +24 V power supply. |
Follow us on