(1)| 6/22/2013 1:08 AM | |
|
Joined: 10/7/2005 Last visit: 1/23/2026 Posts: 3054 Rating:
|
Hello rusli_rusli these type of calls of FB244 and FB245 are the "SEND ALL" and "RECEIVE ALL" calls which need to exist in the program on top of any "direct" Send and Receive calls. Have a look at chapter 11 of the S5-115U Programmable Controller manual for more on this and attached is also a pic from the relevant section. I hope this helps |
|
Cheers |
|
This contribution was helpful to
|
|
| 6/24/2013 4:33 AM | |
|
Joined: 10/7/2005 Last visit: 1/23/2026 Posts: 3054 Rating:
|
Hello rusli_rusli The best advise I can give you is to do more homework to determine and analyse the CP525's configuration (for which you need COM525)and theprotocol in use (e.g. RK512, 3964(R), special driver etc.). The following manuals will come in handy for this task: Manual for S5-CP525 / CP524 / COM525 SIMATIC S5 Special Driver for CP 524 / CP 525-2 (S5-DOS) OPEN DRIVER for Data Link to Host Systems Operating Instructions for Special Driver S5-R00E "STANDARD DATA LINK (RK512) with parameter assignment facility with 3964 / 3964R procedure" Analysingthe PC's configuration may give you clues too, but there's just too many possibility of the type of serial link and protocol in use that you really have to work out the configuration of the CP525. I hope this helps |
|
Cheers |
|
This contribution was helpful to
|
|
Follow us on