(1)| 7/11/2013 3:55 PM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Dear dontxbotherxme You have to check from PLC side only because we don't think you have any issue related to drive Now during stop in such case, check control word received from PLC, and check whether ON command is withdrawn or not Normally First word is used for control word so you can check from para r2090 Regards, Devesh Vithani |
|
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
| 7/11/2013 5:38 PM | |
|
Posts: 4620 Rating:
|
Hi dontxbotherxme, I do not know if it is the same problem that I had long ago, it happened that the motor would stop by itself for no reason, do research and found that the connector between the Micromaster and the Profibus module was not stuck well. Maybe if the PLC has planned for messages maybe you do not realize. is only a suggestion. |
Follow us on