2/2/2013 12:21 PM | |
Posts: 2964 Rating:
|
Hello, What is the HMI version are you using in your Machine ??? May be you are talking on the internal... The start-up data (e.g. NC and PLC) of a control system are stored in a battery-buffered memory. To prevent these data being lost in case of a battery or module fault, a data backup must be performed upon completion of the start-up or after modifying these data. The backup is written on the NC-card. The NC-card is located in the slot for the memory card of the NCU-component group. The data backup can be created for the following ranges: NC PLC The memory capacity on the NC-card is limited. A check should be carried out whether existing archives can be overwritten or deleted. Check the informations for the external.... You should format your PCMCIA with cardware properly and then insert in the machine or if have Compact flash(Format to be done in FAT)with an adapter that can be plugged in PCIA slot in PCU20 this can also be tried.... Check this PDF attachment... Regards, Prakash Attachmentcreating_restoring_backup on PC card.pdf (978 Downloads) |
2/4/2013 4:15 PM | |
Joined: 1/19/2012 Last visit: 9/26/2024 Posts: 20 Rating:
|
I think you are correct about the NC card. I check the screen (see attached pictures). I am not given the choice of PC Card. How do I "enable the software options"? Greg
Attachment20130204_080502.zip (592 Downloads) |
2/6/2013 5:53 PM | |
Joined: 9/10/2007 Last visit: 9/16/2025 Posts: 71 Rating:
|
The option is the same for the network configuration on PCU20(Network/disk drive management). Look the logic drive configuration (attach.). Good luck. AttachmentF:\Logic drives.pdf (725 Downloads) |
Last edited by: Caldas at: 2/6/2013 6:13 PM |
|
Follow us on