(0)| 8/1/2013 11:18 AM | |
|
Posts: 519 Rating:
|
Hot Swap is depends on CPU. . Generally S7-300 CPUs does not support Hot swap. . Also refer this "Module Change During Operation" |
Last edited by: Pranav J. Bhagat at: 8/1/2013 11:32 AMLast edited by: Pranav J. Bhagat at: 8/1/2013 11:25 AM |
|
| 8/1/2013 1:33 PM | |
|
Joined: 4/24/2006 Last visit: 1/23/2026 Posts: 9106 Rating:
|
Hello, You will have to use an "active Backplane" for example: 6ES7195-1GF30-0XA0 ET200M, Rail 530mm And the busmodules: 6ES7195-7HD10-0XA0 ET200M, Bus unit f. 2 IM 153-2 RED or the Redundancy bundle: 6ES7153-2AR03-0XA0 ET200M IM153-2 Red. bundle
And for the I/O modules for example: 6ES7195-7HB00-0XA0 ET200M, Bus unit f. 2 40mm I/O modules Best regards, Wizard |
Follow us on