8/5/2013 4:43 AM | |
Posts: 4 Rating:
|
Hi all, I have a problem with function FB 226(BAS_OP30) when i convert step5 to step 7. In Step 7 FB 226 not available i find document FB226 to know output and what's change in FB 226. Anybody have document about it ?( JU FB 226 ) Thanks for reading (CPU 948) -> (S7-400) AttachmentAttach.pdf (497 Downloads) |
Last edited by: hoa024 at: 8/5/2013 5:13 AMLast edited by: hoa024 at: 8/5/2013 5:11 AM |
|
8/5/2013 10:12 AM | |
Joined: 11/21/2007 Last visit: 7/25/2025 Posts: 2326 Rating:
|
Hi hoa024 What exactly is the error that you are getting when converting this block to S7. ? This looks like a user written block and should be convertibible to S7 without too much trouble ! Cheers Navnag |
There is no such thing as the last bug in a program |
|
8/5/2013 10:33 AM | |
Posts: 4 Rating:
|
I have a source S5 , I use module "Converting S5 Files" to convert s5->s7 FB226 "not available" in s7. I open source S7 after convert and see have comment "CALLL FB 226". I'm not sure my function will be right after convert because i can't find document talk about communication FB226 in step 7. Please see my attach for details Thanks AttachmentAttach.zip (395 Downloads) |
8/5/2013 1:05 PM | |
Joined: 11/21/2007 Last visit: 7/25/2025 Posts: 2326 Rating:
|
Hi hoa024 The Block FB 226 is being identified with the Name : TDOP:L2 It is a standard block required to be called for Communication between a S5 PLC and a TD/OP on L2 Bus. ( Itis Normally numbered as FB 55 ) Pl see the attached details regarding usage of the FB in S5 This block is not at all required in S7 as TD/OP can establish direct communication with the PLC witout having to call any special FBs for TD/OPs. You can therefroe Delete this block ( and associated DB_ZU andrest of the logic programmed to run this block - See the Description attached ) Hope this helps Cheers Navnag AttachmentS5_Std_Blocks_for_TDOP_Profibus.pdf (485 Downloads) |
Last edited by: Navnag at: 8/5/2013 1:06 PMThere is no such thing as the last bug in a program |
|
8/6/2013 5:28 AM | |
Posts: 4 Rating:
|
Thanks you so much Navnag Do you have document about FB standard s5 (FB 120->125 ) ? |
Last edited by: hoa024 at: 8/6/2013 5:29 AM |
|
8/6/2013 6:00 AM | |
Joined: 11/21/2007 Last visit: 7/25/2025 Posts: 2326 Rating:
|
Hi hoa024 FB 120 -> Fb125 are called Data Handling blocks and are used in S5 135U/155U for Controlling communication using Communication processors like CP525 , CP 524 , CP544 etc. In most cases these may not be needed in S7 (e.g. where the CPs are used to establish communication withHMI / SCADA ) and can be ignored. In few cases ( e.g. Modbus / USS Communication ) The S5 Program needs to be manually ported to S7 ( There is no automatic conversion possible ) You can find more details about these blocks in the Manual of the Specific Communication processor for which these blocks are used in the S5 Software. CP 524/525 : http://support.automation.siemens.com/WW/view/en/12806839 CP 544 : http://support.automation.siemens.com/WW/view/en/1108809 Attached pl find an Extract from the Manual of CP544 giving details of the Data Handling blocks as applied to CP 544. AttachmentCP544_Data_Handling_Blocks.pdf (490 Downloads) |
Last edited by: Navnag at: 8/6/2013 12:02 PMManuals Links added There is no such thing as the last bug in a program |
|
Follow us on