(0)| 8/9/2013 2:50 AM | |
|
Joined: 9/27/2006 Last visit: 1/20/2026 Posts: 12481 Rating:
|
Hello Mike; Controlling a MM440 drive over RS-485 implies using the USS protocol (the other option is Profibus-DP, requiring a Profibus-DP master in the S7-1200 and a Profibus-DP slave module on the MM440). Look at the following Application from Siemens and see if it gives you the information you need to proceed: Simple networking and cascading of drives (CE-X8)
What are the differences between USS communications on Sinamics G110 and Micromaster 4?
And the following manual should give you more details on the internals of the USS protocol: Specification: Universal Serial Interface Protocol USS Protocol |
Last edited by: dchartier at: 8/9/2013 2:57 AM |
|
Follow us on