(0)| 8/14/2013 1:43 PM | |
|
Posts: 461 Rating:
|
This might be useful i think MPI + USB cable http://www.fourstar-dy.com/Uploadfile/20101012165012247.pdf Regards, Nelliyan.G |
| 8/14/2013 5:43 PM | |
|
Joined: 9/27/2006 Last visit: 1/20/2026 Posts: 12481 Rating:
|
Hello TKM; you will find connectivity information or WinCC Flexible Runtime systems in the following manual: SIMATIC HMI WinCC flexible 2008 Communication Part 1 For example: The following hardware components are required for inclusion in an existing PROFIBUS DP network: ● To connect a Panel PC or standard PC to the PROFIBUS DP interface of the S7 PLC, you need either a communications processor (for example, CP 5512, CP 5611), or an adapter (for example, PC adapter). PC adapters are available for the RS232 (serial) and USB (USB 1.1) ports. Hardware components required for Ethernet networking: ● To connect a Panel PC or standard PC to the S7-300/400 PLC over Ethernet, you need a communications processor (for example CP 1613, CP 1612, or CP 1512) or Ethernet network card (for example SIMATIC Panel PC On-Board Ethernet adapter, standard Ethernet module). Look also inside this document: SIMATIC HMI WinCC flexible 2008 WinCC flexible 2008 Runtime Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 8/14/2013 5:44 PM |
|
Follow us on