(1)| 8/16/2013 9:04 AM | |
|
Joined: 4/24/2006 Last visit: 1/23/2026 Posts: 9107 Rating:
|
Hello Bargathi, I think you should use PC-Access (OPC server): how can you graphically display a variable of the PLC via EXCEL as OPC client with PC Access as OPC server? Some other links: how do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP243-1) via Ethernet? What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options? Best regards, Wizard |
This contribution was helpful to
|
|
Follow us on