6/6/2013 3:52 PM | |
Joined: 2/4/2013 Last visit: 8/6/2025 Posts: 12 Rating:
|
Hi, The RFID reader with IO-Link interface automatically provides the data read by the transponder (process image of the inputsPII). In doing so, the unique identification number (UID) as well as any application data of a predefined memory area can be read ('Read Only'). No RFID-specific programming is necessary for this. You have only to enter the read-command and the address of the data to be read on the transponder (process image "output" PIQ). See the manual (chapter 5.2 and 5.3.3): http://support.automation.siemens.com/WW/view/en/60641859?Datakey=68014640 An onlineSiemens Example will soon be available for the Reader with IO-Link interface. |
8/19/2013 4:15 PM | |
Joined: 2/4/2013 Last visit: 8/6/2025 Posts: 12 Rating:
|
Hi, See also the new Siemens Application example: http://support.automation.siemens.com/WW/view/en/73565887 With RF200 IO-Link Reader you can only read user data ("Read Only" Reader). |
Last edited by: Valident at: 8/19/2013 4:20 PMLast edited by: Valident at: 8/19/2013 4:19 PMLast edited by: Valident at: 8/19/2013 4:17 PM |
|
Follow us on