(1)| 9/9/2013 8:30 AM | ||
|
Posts: 3 Rating:
|
HelloGanes10, thanks for information,I triedto change the configuration of the RT to V11 and it works, but just withSP2 ofWinCC RT Advanced V11 . ForWinCC RT Advanced V12 SP1, I mean these products: "6AV2104-0BA02-0AH0" "6AV2104-0BA02-0AA0"
|
|
| 9/9/2013 9:13 AM | ||
|
Joined: 8/31/2010 Last visit: 12/6/2025 Posts: 1525 Rating:
|
Hello buonboy, "6AV2104-0BA02-0AH0" - suchproduct / order no.does not exist. Generally there will not be a seperate order number for RT v12 and RT v12 SP1. (after the release of SP1, the 6AV2104-0BA02-0AA0 is delivered with SP1 by default - which means the software is always delivered with the latest service pack andupdate) If you have further doubts, do not hesitate to post 'em. |
|
|
Like it? Rate it! |
||
| 9/9/2013 9:43 AM | |
|
Posts: 3 Rating:
|
HelloGanes10, for the product"6AV2104-0BA02-0AH0",I just found it here: should be the downloadable versione of "6AV2104-0BA02-0AA0": The same for "6AV2104-0DA02-0AA0"and"6AV2104-0DA02-0AH0" with different powertags. But just to be sure, there may be any incompatibility between a project developed by WinCC V12 and then in fuction with RT V11? Or is better to try to have the same version? Thanks. |
| 9/9/2013 9:52 PM | |
|
Joined: 8/31/2010 Last visit: 12/6/2025 Posts: 1525 Rating:
|
Hello buonboy, You are absolutely right. It is the downloadable version. "6AV2104-0DA02-0AA0"and"6AV2104-0DA02-0AH0" are SIMATIC WinCC Runtime Advanced 512 PowerTags V12, whereas one of them is again downloadable version. When you choose the runtime version while creating a runtime, you have to choose whether v11 or v12. If you choose v11 RT, you will be able to make use of the functionalities only which are restricted to v11. Whereas if you choose v12 RT, you will be able to make use of all the latest functionalities including v11 functionalities. As you said rightly, in new projects it is better to go with TIA Portal v12 (WinCC B/C/A/P v12) and WinCC RT Adv / Prof v12. Only if it is necessary to continue the RT version with v11, you have to choose v11 from the drop down box. |
|
Like it? Rate it! |
|
Follow us on