(1)| 6/4/2013 12:26 PM | |
|
Joined: 2/27/2008 Last visit: 11/3/2025 Posts: 1 Rating:
|
Dear all, I need to connect a printer with a TP1200 Comfort panel. I've found the following list (see enclosed) of approved printer by Siemens. But the four Laser (B/W A4 format) printer are no more deliverable, we cannot buy them anymore because these Model are too old.. Do you have a list up-to-date? More recent than March 2012? The TP1200 Comfort panel is running on Windows CE. There's only a few printer running on this OS. Could you give me any other parameter I've to take care before to buy a printer? If I'm using another printer that the printer from the list, how can I send the DRIVERS to the windows CE. Are you using the software HMI tools : SIMATIC ProSave? Thank you very much indeed, AttachmentPrinters_Panels_en.zip (1621 Downloads) |
| 10/9/2013 10:15 AM | |
|
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
New question splitted to Which HP/Cannon laser B/W printer supports SIMATIC HMI TP1200 COMFORT( 6AV21240MC010AX0 )? Best regards O_Moderator |
Follow us on