(0)| 10/20/2013 9:56 PM | |
|
Posts: 895 Rating:
|
... I don`t know the ABB drive, but for extruders I would use a SINAMICS G120 (up to 250kW) or the SINAMICS G130 (also for higher power available). |
| 10/20/2013 11:31 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello Parthiban.R; This Siemens brochure suggests the Sinamics G150 for an extruder: SINAMICS drives - Siemens SINAMICS® G150 is the Siemens drive solution for applications that do not require regenerative feedback into the line supply. These are predominantly applications with square-law load torque characteristics – i.e. pumps, fans and compressors, but also constant-torque applications such as extruders, mixers and crushers. voltage rangesSINAMICS G150 Power and voltage rangesSINAMICS G150 380–480 V 110–900 kW 500–600 V 110–1,000 kW 660–690 V 75–1,500 kW Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/20/2013 11:32 PM |
|
Follow us on