(1)| 8/1/2007 8:42 PM | |
|
Posts: 8 Rating:
|
Just to inform the problem is solved, It was a firmware in the CP1430TF cards in the PLCs that does not show when you are using a CP1413 in the PC but when you change to a CP1613 it just happens. The correct firmware versions for the Cp1430TF cards in the PLCs you can checkit with the attached document extracted for Simatic net support. As an additional information, the problem occurs equally with the old CP1613 (A1) in the PC as with the new CP1613 (A2), and solves equally changing the firmware in the CP1430TF card in the PLCs. A lot of Thanks to Nemo and J_Bell for your support, this was one of these weird problems that without prior experience is very difficult to pinpoint. Regards, Juan A. Camalich Chilamac AttachmentCP1430 Firmware Upgrade v309.pdf (229 Downloads) |
Follow us on