(0)| 11/18/2013 5:59 AM | |
|
Posts: 4620 Rating:
|
Hi MJRVSV, To see if the HMI communicates with the PLC can use the life bit. In the HMI go to Connection then Coordination, there is another line which is called Coordination. Take a look: Monitoring the connection between a panel and the control |
| 11/18/2013 1:19 PM | |
|
Posts: 166 Rating:
|
Thanks for ur reply Pl refer to step 7 program Please advice cani just add call FC118 in OB1 then Create FC118 and copy contents of FC1 in lifebit onto FC118 Create DB158 , copy contents of DB1 of lifebit onto DB158 then download to PLC and check will it be correct to do so as FC118 and DB158 not in use so far Pl advice Regards, AttachmentUpload_m.zip (94 Downloads) |
Follow us on