(1)| 7/1/2007 12:03 AM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi, The CP 342-5 only supports DP V0 slaves. In the STEP 7 Hardware Configuration, DP slaves that are to be operated on the CP 342-5 are configured only from the catalog folder "PROFIBUS DP > DP V0 Slaves". If the DP V0 slave has been incorporated via a GSD file, it has to be configured from the catalog folder "PROFIBUS-DP > Other Field Devices". |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
| 11/12/2007 5:19 AM | |
|
Posts: 7 Rating:
|
Thankyou master, anyway how can I use "Acyclic Send Data"? |
| 11/12/2007 1:45 PM | |
|
Joined: 8/25/2005 Last visit: 1/14/2026 Posts: 1162 Rating:
|
Hello Dian, which DP-Master are you using? The CP 342-5 doesn't support acyclic communication Sabine |
| 11/29/2013 10:31 AM | |
|
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
New question splitted to communication between simocode pro and plc 315 2 pn/dp Best regards O_Moderator |
Follow us on