(0)| 12/3/2013 2:36 PM | |
|
Posts: 166 Rating:
|
Dear ALL , I was using Siemens Sample Program in which the Google api in HTML was mapped with wincc TIA . Micro Automation: Wireless Tracking with GPS based on GPRS - MAS 41 https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objid=31745883&nodeid4=20229805&nodeid0=46635999&switchLang But when the coordinates are being refreshed , the whole screen is getting refreshed everytime so that lead to refresh and reloaading of map everytime ( I think to centre the Marker ) , that is making map not seen clearly to the observer . Can any one tried using it and found this issue ? If Yes , then How was it resolved ? Thanks Sarabjot Singh Manku |
| 12/6/2013 1:44 PM | |
|
Posts: 1299 Rating:
|
Hello, in the example you posted they use wincc flexible. did you migrate the project to tia? K!ke |
| 12/7/2013 9:37 AM | |
|
Posts: 166 Rating:
|
Yes K1ke . |
Follow us on