(0)| 12/26/2013 5:02 AM | |
|
Posts: 163 Rating:
|
Hi, I have a CPU 314c-2PN/DP and CU 240E-2DP connected on industrial ethernet. I have configured the drive and CPU in hardware and downloaded successfully but there is SF and BF on the CPU as well as on CU. Both CPU and drive are accessible so there is no issue with ethernet connectivity and IP address assignment. I have also attached the file of diagonstic buffer with this thread. Pls help as soon as possible. Regards, Rudrani.
AttachmentModule Information.pdf (335 Downloads) |
Follow us on