1/10/2014 12:44 PM | |
Joined: 10/11/2006 Last visit: 9/15/2025 Posts: 6040 Rating:
|
Dear flako, FW 3.x was with MASTERDRIVES Vector Control (CUVC) FW 2.x is with a MASTERDRIVES Motoin Control Performance 2 (CUPM). Between both, CUVC - CUPM,the parameter adjustmants can not used toeach other. (Comletely different). For parameters from CUVC FW3.2 to 3.4 a so called delta upload from FW3.2and then download to FW 3.4 device, which has been in default before is a good way. Please find the differences for CUVC here : http://support.automation.siemens.com/WW/view/en/23958763 |
With best regards, |
|
Follow us on