(0)| 3/5/2014 11:38 PM | |
|
Joined: 11/26/2013 Last visit: 5/16/2025 Posts: 4 Rating:
|
Hello, I desperately need some help with my 4DE02-0AB0 1count5V module. Im trying to connect a concens actuator that returns 2 5v hall sensor signals (see datasheet). The A and B signals are connected to the A and B terminal on the 4DE02 countermodule. In the hardware configuration i tried multiple settings. loaded a program as descibed in the ET200s technogical functions document. A #SW_GATE = DB50.DBX 4.0 A #SET_HOME_POS1 = DB50.DBX 5.0 //Write to the control interface L DB50.DBD 0 T PQD 500 L DB50.DBW 4 T PQW 504 //Network 3: Read from the feedback interface L PID 500 T DB50.DBD 8 L PID 504 T DB50.DBD 12 No i dont get a change in the actual position when operating the actuator We got a change in the actual position when we connected a few relais so we can invert the A and B signals and connected these to the /A and /B terminals (obviously not fast enough) Is it possible to get the count module to work when i am only using the A and B terminal on the count module? In the VAT table i see a high boolean on feedback word bit 3 (Bit 3: Short circuit / wire break / encoder signal) when i only connect the A and B terminal Hope you can help me out Regards Johan Muurling Attachmentdata-sheet-hall-concens-ver3-oct-2010-uk_0_0.pdf (334 Downloads) |
Follow us on