(0)| 4/10/2014 9:26 AM | |
|
Posts: 3 Rating:
|
We have 1 no goliath crane which, have two trolleys(Upper trolley& Lower trolley), 4 nos hoists (MH1,MH2,MH3 &AH), and 2 nos leg(Fixed leg & Hinged leg). All the drives are connected to Simotion D435 and two control extentions. The crane has been commissioned on dec 2012. Now a days some faults which are coming frequently in drives specially when the crane is not working/stand by mode(approx. 6-8 hrs after operation). The faults are: 30885,30851,30837,30845 After fault occurs we do only power recycle and the respective drives becomes healthy. Checked all drive cliq tight ness,routing ,electronic earthing, DC Voltage all are found OK. What to do? PLZ help Attachmentdrive grse.pdf (140 Downloads) |
Follow us on