4/21/2011 7:43 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Dear All, In one of my S7200 PLC Project , i am using EM231 8 channelAI card having MLFB number is 6ES7231-0HF22-0XA0. i want to configure first six channel as voltage signal and last two channel as current signal. as per the datasheet of the module last two channelcan be configured as current signal. i read the dip switch setting of the module and did the setting as mentioned but i didnt get desire output from the module. please find attached sheet for your reference. can anybody tell me the dip switch setting in this case? Thanks in advance. AttachmentEM321 DIP SWITCH SETTING.zip (708 Downloads) |
VANDE MATARAM..... |
|
7/3/2014 9:25 AM | |
Joined: 3/25/2013 Last visit: 4/7/2025 Posts: 176 Rating:
|
New question split intoEM 231 Analog Input Card - which dip switch to change. With best regards, Narrator1
|
Follow us on