5/27/2014 10:42 AM | |
Posts: 291 Rating:
|
Hello C.kt, Don't worry!! .xls is supported to upload event in Client and Server Structure (also supported among a Web Server and Client!! Because I take a .xls as a Datasource (including Table) and access it through Jet Engine, so actually you don't need to have Excel Application installed in your Server or client. ***** In fact, I just wanted to know the TagNames mapping to each "cells" for displaying. ;-) Thank you for that you've attached the sample layout you want. In order to avoide difference of the platforms between yours and mine, I'd like to take use of OWC-Spreadsheet to: 1. Get the corrent tags' value and show them in the OWC-Spreadsheet according to corresponding cells. 2. User can do some input on cells but those input won't be applied (set) to TagValue immediately. 3. There will be a "modify/ confirm" button aside, after pressing that ~ the modification/input will be set to the real TagValue. But... please do me a favour first! Please try to open the attached .pdl and see if you can see the OWC-Spreadsheet inside in RT. I think you'll need to install OWC component in advance before doing the project conversion. Best regards, Komi AttachmentTest.zip (387 Downloads) |
Last edited by: Komi at: 5/27/2014 10:43 AMMany typos fixed :D |
|
This contribution was helpful to
1 thankful Users |
7/10/2014 11:48 AM | |
Joined: 9/1/2005 Last visit: 8/22/2025 Posts: 4114 Rating:
|
Follow up question published by MauricioRCis split to a seperate thread with the subjectSecond Duplicate: How can I create a table and a graph in WinCC with my data?. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on