(0)| 7/10/2014 7:21 PM | |
|
Joined: 5/10/2007 Last visit: 9/27/2025 Posts: 14 Rating:
|
I have a problem with trend view in WinCC Flexible 2008 SP3 Upd4. I've made a project with data log and I've added a tag that is logged each 5s. I've configured trend view to display logged data and when I open screen in PC RT for example in 8:10:35 AM displayed data is unitl this hour. After that trend stayed freeze and doesn't update data. If I want to update data I have to use buttons for scrolling trend. I want trend view to be refreshed automatically like real time trend and to show log data. I've done this with older version 2005 and works fine, but with last version I can't make it work. In the attachment is the project which I created. Please help. AttachmentTestProject.zip (336 Downloads) |
Follow us on