(0)| 7/23/2014 3:23 PM | |
|
Posts: 4620 Rating:
|
Hello juliaf, The code of the motor with Z, I remember the final means that it has something special, right? can you tell us what? What application do you need? And something complex (maybe it's better SINAMICS) or, for example, is only a conveyor belt? Your inverter is unfiltered then maybe you need to mount the filter and mains reactor. and please have a look for 50/60Hz: 50 Hz to 60 Hz i nUS.... and thinking as you say is a new line I would think more like a Sinamics that a Micromaster I think that in a short time will go into a discontinuation phase: Siemens Industry Online Support - Automation Service, Automation ... |
Last edited by: Ste39 at: 7/23/2014 4:30 PMLast edited by: Ste39 at: 7/23/2014 3:24 PM |
|
Follow us on