8/4/2014 6:06 PM | |
Posts: 7 Rating:
|
I have an existing machine with a defective analog module. Can I simply swap this in without the program or Micro/Win? |
8/4/2014 8:04 PM | |
Posts: 7 Rating:
|
Thanks, that should be an RTFM question, but I didn't find it anyplace. |
8/4/2014 10:21 PM | |
Posts: 5225 Rating:
|
Hi there. Seeing the title, I am little worried.. Do you wish to change one of the external cards with another one, or do you wish to exchange the analog input that is onboard to the CPU? Giving a part number (of the analog card) would be helpful if futher enquiries develop. For the System Manual for the S7-200: [LINK] Put your attention the the Appendix section for hardware descriptions. These are VERY detailed. Let us know if there is more our community can help you with. w |
8/13/2014 1:51 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
New question split to COMPARE and MOVE instructions. Best regards O_Moderator |
Follow us on